Operating System on imx6ulevk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Operating System on imx6ulevk board

691 Views
nitigupta
Contributor I


Hello All,

Currently I am working on imx6ulevk board having configuration "140kB RAM, 1MB ROM, 524 MHz One core cortex A7 with Neon & 1MB QSPI flash(external)". I want to run either linux or rtos on it but I am not getting which linux or rtos I should use on it. Is it feasible to run linux on it. Also I am confused which rtos is best possibly work with it.

Any help in this regard is highly appreciated.

Thanks,

Niti Gupta

0 Kudos
Reply
1 Reply

488 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niti

for linux one can look at i.MX6UL product page:

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul)

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

i.MX6UltraLite Evaluation Kit|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply