Hello all,
On my custom board based on i.Mx6s , I've made a Yocto Dizzy 1.7.3 image with command
bitbake fsl-image-multimedia-full
The system starts, and al seems working fine. Now I'm trying to capture image from camera with command:
gst-launch-1.0 imxv4l2videosrc device=/dev/video0 input=0 ! imxipuvideotransform ! fakesink
But it returns
WARNING: erroneous pipeline: no element "imxv4l2videosrc"
and command stop the execution.
Please can you help me to understand and fix the problem?
Thanks for all
Luigi
Hi Luigi
imxv4l2videosrc is from community Gstreamer-imx plugins,
(one can post qustion for it to meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale)
Also suggest to look at similar discussion on :
IMX6 ADV7180 GStreamer1.0 (tvsrc substitute)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------