Hi,
I,test the snvs-pwrkey drive for I.MX6UL, I found the long press ONOFF not shut down,but there are interrupt is generated
Have any Suggestions? Is there a link with the hardware?
Hi 小辉哥 в
on Sabre schematic spf-27392 p.19 "AUTO ON" feature is used, to turn it off
it is necessary to implement "Optional : PMIC Power ON circuit"
Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files. (REV C5)
SABRE for Smart Devices Reference Design|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi,igor,
I'm sorry, I forgot to use processor, I use a imx6ul, not imx6Quad, Schematic is also reference imx6ul - EVK
please check that you have valid coincell connected
thanks, i have valid coincell connected, found the reason is caused by the reset chip, I use a UM811, UM805RE instead.