USB on i.MX6UL without external +5V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB on i.MX6UL without external +5V

Jump to solution
493 Views
jsopenrb
Contributor II

Is it possible to run USB in host-only mode without +5V on USB_OTGn_VBUS? Can we power internal USB block with +3.3V?

Labels (1)
0 Kudos
1 Solution
404 Views
igorpadykov
NXP Employee
NXP Employee

Hi J

yes, for correct operation of USB module, LDO_USB should be

powered with USB_OTGn_VBUS with value 4.4-5.5V according to

Table 10. Operating Ranges i.MX6UL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards

igor
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
405 Views
igorpadykov
NXP Employee
NXP Employee

Hi J

yes, for correct operation of USB module, LDO_USB should be

powered with USB_OTGn_VBUS with value 4.4-5.5V according to

Table 10. Operating Ranges i.MX6UL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos