hi,
I alreday design sch. of IMX6Q(MCIMX6Q5EYM10AD),now I need to let sch of IMXQ6Q compatibity with IMX6DUAL-LITE(MCIMX6U5EVM10AC).It means that I can solder IC IMX6Q or IMX6DUAL-LITE on the same PCB board.
what is the detailed difference between IMX6Q and IMX6DUAL-LITE ON sch? Give me the doc
or sch-demo,thanks.
Hello,
Please refer to AN4397 : “Common Hardware Design for i.MX 6Dual/6Quad
and i.MX 6Solo/6DualLite”
http://cache.nxp.com/files/32bit/doc/app_note/AN4397.pdf
Also, You may look at the following design
SABRE|Automotive-Infotainment|i.MX6|NXP
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI,
thanks.
1:I read "http://cache.nxp.com/files/32bit/doc/app_note/AN4397.pdf",but what is meaning offollowing?
The IMX6Q/DUAL also support SD/MMC boot mode. see follow picture.
Hello,
SD/MMC Manufacture mode is special feature, that provides (secondary) boot,
when (primary) boot failed. Please refer to section 8.11 (SD/MMC Manufacture Mode)
of the i.MX6 S/DL RM.
Regards,
Yuri.