The copy of Suite56 that is available for download has indeed not been updated for
a very long time. It has also been superceded by a whole new development tool
suite: Symphony Studio. Please be aware, however, that there is no telling how
much longer Suite56 will remain available for download.
You may obtain more information about Symphony Studio from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SYMPH_STUDIOThe new suite is based on the open-source framework Eclipse. The graphical
GDB debugger in Eclipse connects to a port of the command line GDB for the
56300 architecture. Connection to target hardware is made through a remote
GDB server on the local machine (but it is not required to be, allowing for remote
debugging). The built-in server is OpenOCD which allows the use of parallel
port-JTAG adapters as well as several FTDI FT2232-based USB-JTAG adapters.
One such USB adapter is built directly onto the Symphony SoundBite development
board, a new development board that was released late last year. See more info at:
http://www.freescale.com/symphonysoundbiteThe Symphony SoundBite is a totally self-contained board with an MSRP of $150.
While it is not as flexible as the DSPAUDIOEVMMB1 and associated daughter
cards, it is much more affordable.
--david