Hi,
We are trying to setup IMX6Q-SDB with Linux L3.14.52_1.1.0-ga_images_MX6QDLSOLO using L3.14.52_1.1.0_ga-mfg-tools from Windows 7. We are trying to install it on to eMMC. We are monitoring it in Hyperterminal. Progress stops at a point and the last message we receive is "random: nonblocking pool is initialized". We are quite new to this and any help on this is appreciated. I am attaching the terminal log, cfg, vbs and ucl2 files.
Thanks in advance.
DER
Original Attachment has been moved to: ucl2.xml.zip
Original Attachment has been moved to: mfgtool2-yocto-mx-sabresd-emmc-1.2g.vbs.zip
Original Attachment has been moved to: Install-Log.TXT.zip
Original Attachment has been moved to: cfg.ini.zip
Hi DER,
Have you ensured that you used the proper files and/or are the files placed on proper directories?
I just downloaded MFGTool for Yocto 3.14.52 (L3.14.52_1.1.0_ga-mfg-tools.tar.gz), and the Yocto image was properly downloaded to eMMC, and then, the SABRE SD board booted properly.
The script that I have used is the following:
\L3.14.52_1.1.0_ga-mfg-tools.tar.gz\L3.14.52_1.1.0_ga-mfg-tools.tar\mfgtools-with-rootfs.tar.gz\mfgtools-with-rootfs.tar\mfgtools\mfgtool2-yocto-mx-sabresd-emmc-1.2g.vbs
Hope this will be useful for you
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------