Dear All.
I'm trying to install Ubuntu 14.04.4 core on i.MX6SX Sabre board.
Attached File is the shell script for installing toolchain-4.9-2014.09, u-boot-v2015.04_3.14.52_1.1.0, linuxkernel-3.14.52_1.1.0 and ubuntu-core-14.04.4.
Procedure of attached shell script)
1. Downloading toolchain-4.9-2014.09.
2. Downloading and building u-boot-v2015.04_3.14.52_1.1.0 source.
3. Downloading and building linuxkernel-3.14.52_1.1.0 source.
4. Preparing SD.
5. Installing u-boot and kernel image files on SD.
6. Downloading and install ubuntu-core-14.04.4.
As follows, it stopped at "Stopping System V runlevel compatibility [ OK ]".
I attach the shell script and log file.
Can you help-me?
--------------------------------------------------------------------------------
U-Boot 2015.04 (Feb 23 2016 - 23:51:46)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 35 C
Reset cause: POR
Board: MX6SX SABRE SDB
........................................................................................
........................................................................................
* Starting Mount network filesystems [ OK ]
* Stopping Failsafe Boot Delay [ OK ]
* Starting System V initialisation compatibility [ OK ]
* Starting configure virtual network devices [ OK ]
* Stopping Mount network filesystems [ OK ]
* Stopping System V initialisation compatibility [ OK ]
* Starting System V runlevel compatibility [ OK ]
* Starting save kernel messages [ OK ]
* Starting regular background program processing daemon [ OK ]
* Stopping save kernel messages [ OK ]
* Stopping System V runlevel compatibility [ OK ]
------------------------------------------------------------------------------------------------------------
Original Attachment has been moved to: log.txt.zip
Original Attachment has been moved to: imx6sx_sabresd_3.14.52.sh
I haven't tested the same procedure as yours, but I found some helpful document to you for reference