Dear sir,
Using this i.MX6Q device , Slip mode (LVDS) and HDMI of mirror display or is possible ??
This is very difficult problem.
LVDS= 1920x1080, HDMI=1920x1080, OS: Yocto project
Y.Yatsukura
Dear Igorpadykov
I'm sorry. "Slip " instead, is the "Split" is correct.
I use 1920x1080(2 port LVDS) Panel LCD.
Thanks.
Best regards
it may be useful to look at L3.10.31_dual_channel_lvds.patch.zip
https://community.freescale.com/message/525359#525359
~igor
Hi Yatsukura
what do you mean by "slip" ? Some mirror examples can be found on
https://community.freescale.com/thread/313507
Re: Dual Display setup on Yocto build
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!