I’m looking at the details of specifically which T1040 we use. I could put a part number together for exactly what I want, but I want to make sure I’m not ignoring a nearly identical variant that is more readily available in distribution and will cause me less headaches to procure.
According to our internal products database, lead time is the same for all currently available T1040 partnumbers, so I do not see a difference which partnumber to order.
Not all possible package options combinations are valid partnumbers, partnumber T1040NXN7PQB is not available.
Please refer T1040 Product Page, "Buy/Parametrics" tab for full list of valid partnumbers.
QorIQ T1040 and T1020 Multicore Communication|NXP
Relative prices are also shown at this page for comparison.
Sorry, partnumbering information is unclear regarding C4 bumps, actually option "7" means 7 = "FCPBGA C4 Pbfree", there are no other options for T1040 partnumbers, all partnumbers come with "7". The "C4" is not an option, this is a part of description "FCPBGA C4 Pbfree", sorry for confusion.
Silicon revision 1.1 is revision we are currently shipping, revision 1.0 is no longer manufactured.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------