Hello Everyone,
Is there any plan to upstream the QorIQ linux NXP branch into the main line linux kernel(kernel.org)?
I very new to this soc's and it is very important for me to work with the main line kernel.
I couldn't found this Architecture LS102x and other LS at the kernel.org site.
What specific chip are you looking for? There are significant differences among chips labelled LS102x. Assuming LS1021A (or related chips LS1020A/LS1022A), that chip support is upstream. What haven't you been able to find?
"Assuming LS1021A (or related chips LS1020A/LS1022A), that chip support is upstream "
Under which path Can I find it?
Related to LS1043, I understand it is too early to be upstreamed… but maybe anyone can guess when it might occure?
arch/arm/mach-imx/mach-ls1021a.c among other places. Grep for SOC_LS1021A
An LS1043A device tree is upstream. Use ARCH_LAYERSCAPE with it. Datapath support and probably some other features are not yet upstream.
Great!
Now I found it.
Tell me… do NXP has an official site that mark which package is already in mainline and which package is not?
For example, see the link to Xilinx Zynq soc:
http://www.wiki.xilinx.com/Linux+Drivers
Thanks
Unfortunately we do not have a site like that.
Hi Alon D,
The QorIQ linux in SDK is always upstream to main line kernel, but main line kernel does not always contain the newest patch in SDK. Because as you know any patch from SDK needs to be discussed and approved before the upstream, but SDK is growing and have it's versions public constantly... And so does main line kernel
Regards
Lunmin
Hi Lunmin,
Thanks for the quick answer,
I am not sure I understand.
1. You say that "The QorIQ linux in SDK is always upstream", so where can I find it?, in which directory in the kernel.org site?
I've check the: Linux/arch/arm path and around, and couldn't find.
2. If the answer is NO. Is there any plan to upstream the kernel? I know that the SDK has its own community and versions, but I need to merge into the mainline.
3. If it is not mainlined, how can I use patches ?(that created for mainline kernel)
4. the SDK linux version is 3.19 while we are now around 4.4, is there any plan to move on?
Best regards,
Alon