When will the KDS support the eMMC interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When will the KDS support the eMMC interface?

478 Views
calvinday
Contributor III

I am using the K66 and would like to interface it to an eMMC device.

0 Kudos
Reply
1 Reply

331 Views
miduo
NXP Employee
NXP Employee

Hi,

There has no plan to support eMMC with KDS. Anyway, you can use the K66 SDHC module to interface an eMMC device. we do have a code example for SD card using MQX, you can find the example code in the following MQX installation folder:

C:\Program Files\Freescale\Freescale MQX 3.8\mfs\examples\sdcard

0 Kudos
Reply