BSC9132 customized design giving reboot problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSC9132 customized design giving reboot problem?

914 Views
manjanagoudapat
Contributor III

with power supply on/off it will boot properly but when i do reboot in the linux command prompt it will print

NAND boot... WARNING: ECC not checked in SPL, check board cfg

Error: SVR = 0x86180311 corresponds to unknown CPU type. Stopping further boot

### ERROR ### Please RESET the board ###

with power supply on / off it will print

NAND boot... WARNING: ECC not checked in SPL, check board cfg

U-Boot 2011.06.913x_WUSDK_1.6 (Feb 13 2016 - 12:03:34)

CPU0:  BSC9132E, Version: 1.1, (0x86180011)

Core:  E500, Version: 5.2, (0x80211152)

SVR is changing in reboot what might be the problem.

please help me out in debugging this problem.

Thanks and regards

patil m

Labels (1)
0 Kudos
Reply
3 Replies

738 Views
ufedor
NXP Employee
NXP Employee

Ensure that all notes after the BSC9132 QorIQ Qonverge Baseband Processor Data Sheet, Table 1. BSC9132 Pinout Listing are fulfilled – i.e. that neither of mentioned signals is floating.

Please provide the processor connection schematics for inspection.

0 Kudos
Reply

738 Views
manjanagoudapat
Contributor III

hello ufedor

in the design whatever you said is taken care,

but why this svr is changing from SVR = 0x86180011 to SVR = 0x86180311 when i do the reboot.

0 Kudos
Reply

738 Views
ufedor
NXP Employee
NXP Employee

This could be caused either by a floating pin (manufacturing defect) or by a bus hold function of an external component.

0 Kudos
Reply