When I'm debugging my code and I open the Disassembly window, it doesn't do anything. I can hit pause or hit a breakpoint for example, and then hit the Disassembly window's home button which is supposed to display the disassembly at the program counter, but it just shows this:
......... ...
And that's it. Refresh does nothing, none of the other buttons do anything either. Ideas?
Hi Robert,
yes, I have seen this sometimes as well. I believe it is related to some race conditions at debugger startup (which thread/context to use), see Bug 337376 – Disassembly view sometimes doesn't update if pinned to a debug context . It is not directly related to KDS as the same problem occurs with Eclipse Luna too. The workaround I have used is to close the view and re-open it with Window > Show Views menu.
I hope this helps,
Erich
That workaround doesn't work for me (KDS 3.1.0).
Hi Robert,
strange, this always helped on my side. Could you post a screenshot? I believe it depends on where your program counter is, so does it fail as well if your program has reached main()?
Erich
Hi there,
just faced the issue with S32DS for PPC and Erich, your workaround did the trick.
Regards,
Ludwig