i am using Mk70
in that how to load my code into cache memory...
is there any sample code
Hi Dhanalakshmi Sreenrama,
Do you just want to download your code to the K70 flash?
What the K70 board you are using now? TWR-K70F120M?
The sample code for TWF-K80F120M, please download it from this link:
Kinetis 120MHz bare metal sample code
Besides, tell me which IDE you are using? Then I can give you a picture shows how to download the code to the board.
Wish it helps you!
If you still have question, please contact with me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------