I'm using PE in KDS to configure the USB in HID mode without external crystal.
It is a custom board using the MKL27Z256VLH4, the board is powered by the usb bus.
I use J-Link to debug. On Linux I got enumeration error, on Windows the same.
Here is the components that I'm using:
MCG Lite mode: HIRC
Core clock: 48 MHz
Bus clock: 24 MHz
USB Clock: IRC48M
I didn't touch in any generated files, is it supposed to work just grabbing the components and configuring them to the project?
I have no experience with KDS and PEx, am I missing something?
I installed the KDS 3.0.0 and upgraded it using "Check for updates" inside it, after that I applied the eclipse update from KSDK 1.3.0.
Attached is the project.
If someone has a *simple* example of the thing working for this micro, I'd appreciate.
Thanks!
Original Attachment has been moved to: test.7z.zip