JenNet-IP and web resources

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JenNet-IP and web resources

1,159 Views
mguc
Contributor II

Hello everyone

I imagine the following setup and functions which I try to realize with JenNet-IP and I'm wondering if it's possible and what would you suggest or change:

Basically, I'm using two nodes (JN5168), one functioning as a border router (connected to a host, like raspberry) and the other as a remote control (typical node). The remote control should be able to trigger some actions by calling a REST interface e.g. http://[ipv6 address of the border router]/my/super/action on the host. As far as my understanding goes, the JenNet-IP does not provide any high level interface/protocol calls for HTTP, CoAP etc. Correct me if I'm wrong. One solution I think of is to implement a "proxy service" on the host/border router, but I would be happy if I could avoid it. If I can't, how could I implement the proxy using the JenNet-IP stack? Is the JIPweb the way to go? Thank you for your help!

With kind regards

Marko

Labels (2)
0 Kudos
Reply
1 Reply

725 Views
EarlOrlando
Senior Contributor II

Hello!

Thank you for your interest in NXP products.

We are happy to support you through our communities, unfortunately we temporarily have a community structure with two parallel systems which has probably not guided you correctly.

Be ensured we are working on fixing the navigation and the offering as soon as we can.

In the meantime, please re-post your question into the monitored space for this product line:

https://nxpcommunity.force.com/community/CommunityForumQuestionList?category=ZigBee

You may find the following page helpful for navigating to the right spaces:

http://www.nxp.com/support/communities:COMMUNITIES

We apologize for the inconvenience,

The NXP Technical Support Team

0 Kudos
Reply