I'm having a problem where a small subset of boards utilizing the MC13234 end up with an LO unlock condition (as indicated by the STATUS2 register). It seems that maybe 1/100 boards will exhibit this condition, and the condition usual presents itself within the first 50 or so transmissions, and is repeatable when the boards are reset. The other 99/100 boards never seem to present the LO Unlock condition.
I'm wondering what exactly the LO unlock means as it pertains to the performance/reliability of the device. Is this sort of a normal thing to see every once in a while, and I should just reset the radio and continue as normal, or can it be indicative of a bigger problem? Are there external factors that can increase the likelihood of LO unlock (e.g. a swapped component leads to an improperly impedance matched antenna port)?
Thanks,
Matt
Hello Matt,
The RF PLL Unlock Condition is very unusual. My advice is to use our reference designs as a hardware starting point, or if you have and the unlocks are occurring, I suggest looking to solder problems.
Please verify that the xtal is working properly in the boards that present this failure.
I will be looking forward to your reply. For further assistance please do not hesitate to contact me. I will be glad to help you.
Best regards,
Earl Ramírez.