Hello,
I am trying to compile Yocto Linux with the nfs-server feature. I want to be able to mount my imx6 sabre board into my development computer for file sharing purposes.
I boot from an sdcard and I bake the core-image-base.bb recipe. When I add the feature nfs-server to the recipe file (IMAGE_FEATURES +="splash nfs-server") it compiles fine but when booting i get:
"INIT: version 2.88 booting
INIT: No inittab file found
Enter runlevel:"
to which nothing happens even when I enter any number.
Can anybody point me in the right direction? What am I doing wrong here?
Thanks in advance for your help,
Jacob
Hi Alejandro,
thank you for the document. I don't really want to boot from NFS but I just want to install the NFS server on my board but boot from an SDcard.
I added the nfs-server to EXTRA_IMAGE_FEATURES and nfs-utilities to IMAGE_INSTALL_append in my local.conf file and the board is booting from the SDcard but now I get that NFS daemon is not supported by the kernel. Do you have an idea how can I solve this one?
Thanks again,
Jacob
Now I get it. I have not tried that out. Let me reproduce the problem on my side. I will keep delving into it.
/Alejandro
Thank you Alejandro, I hope you find something I will also keep looking.
Jacob
Hi Jacob,
Have you checked this document?
i.MX Create NFS Server and Export USB Drive: Yocto Project Distribution
I believe it can be very helpful.
Best Regards,
Alejandro