I was wondering whether the new PE code generated using KDS 3.0.0 for the K65 processor can be considered thread safe? As an example, if I have two threads running at different priorities and one uses i2c1 and the other uses i2c2, will the PE generated code be thread safe since the i2c components are sharing functions in the SDK?
Thanks,
Elizabeth
Solved! Go to Solution.
Hi Elizabeth,
Yes the KSDK_1.3 code is thread safe.
PE is actually only used to generate configuration structures that are used by the static code/drivers in the KSDK.
Regards,
David
Hi Elizabeth,
Yes the KSDK_1.3 code is thread safe.
PE is actually only used to generate configuration structures that are used by the static code/drivers in the KSDK.
Regards,
David
Thank you very much!
Elizabeth