Is it possible load and execute Linux kernel from MQX? Is there an MQX based bootloader that ran launch Linux? I know there is RedBoot (based on eCos RTOS) which can do it
Hello,
Check the below thread and please let me know if this helps!!
Using U-boot as MQX bootloader
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi soledad,
Well actually I had this as an under-question, I wanted to know if I can avoid using U-boot.
What I would want is a bootloader (hopefully based on MQX.. (what does MQX use to load itself, I havent studied) which can load MQX
or Linux, and be royalty free or non restrictive license so that one can modify the sources without releasing custom changes.
Hi,
Unfortunately we at this moment we don't have a solution like you need.
Sorry for any inconvenience.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------