Hi,
I am using FreeRTOS integrated into Processor Expert and implementing it on K20 device.
How should I go about implementing a microSD interface with FAT file system.
Any comment will be highly appreciated
Zohar
Hi Zohar,
you can use it either way: You can use only the SDK (there is a FatFS example in the SDK), or you can use the SDK with Processor Expert (but then it only suppports the fsl_* components), or you can use Processor Expert with the 'non-SDK' components. So you have freedom of choice :-)
Note that the FreeRTOS in the SDK is an older one (8.2.0) while the McuOnEclipse component is using the latest FreeRTOS (8.2.3).
I hope this helps,
Erich
Hi Zohar,
I'm using FreeRTOS with FatFS in several projects, see FatFs | MCU on Eclipse . There are sources/examples available on GitHub (see the links in the articles).
I hope this helps,
Erich
Hi Erich,
As usual, thank you for the fast reply. The link you have send me is using the KSDK 1.2.0. I am using the freeROTS extention, which is not using the SDK. Is it going to be a problem or I can add the KSDK in processor expert?
Thank you,
Zohar