i have a imx dual board with linux-imx 3.10.17 . I want to use weston with wayland as a backend.
I am using yocto for building kernel and rootfs. I enabled DISTRO_FEATURES="wayland" and also made backend = "wayland"
Now I wish to run weston on my board, For this i used command
weston --backend=wayland-backend.so --no-config
It shows me following error:
[19:40:10.197] weston 1.6.0
http://wayland.freedesktop.org/
Bug reports to: https://bugs.freedesktop.org/enter_bug.cgi?product=Wayland&component=weston&version=1.6.0
Build: 1.5.93-5-g2858cc2 configure.ac: bump version to 1.6.0 (2014-09-19 13:40:14 +0300)
[19:40:10.200] OS: Linux, 3.10.17-1.0.0_ga+g33597e3, #2 SMP PREEMPT Fri Oct 23 09:51:35 IST 2015, armv7l
[19:40:10.204] Starting with no config file.
[19:40:10.207] Loading module '/usr/lib/weston/wayland-backend.so'
[19:40:10.339] failed to create display: No such file or directory
[19:40:10.343] fatal: failed to create compositor
What could be the possible reason for this?
-Thanks
Sharvari Harisangam
Hi Sharvari,
If in any case you are using any i.MX6 with GPU you need to apply a Wayland patch in order to avoid build breaks. However I do not sure if these patch work on 3.10.17, probably you will have to upgrade to 3.14.28 BSP.
https://lists.yoctoproject.org/pipermail/meta-freescale/2015-July/014614.html
regards