How can I build system file with ppp in it.
Now I used the command MACHINE=imx6ulevk source fsl-setup-release.sh -b build-x11 -e x11
bitbake core-image-base.
but no pppd in system file of the image. and no /etc/ppp too,
who can help me, what command can build image with ppp,
thank you very much
Hello Tony Zhou,
The ppp package is not installed on the BSP release images as it’s not supported on the BSP but you may add it using the following command on the conf/local.conf file inside your build directory.
IMAGE_INSTALL_append = “ ppp”
I hope this helps.