1080p HDMI and LCD simultaneously on i.MX6D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1080p HDMI and LCD simultaneously on i.MX6D

621 Views
kirgene
Contributor II

Hello,

I'd like to use two 1080p HDMI displays simultaneously, one connected directly to HDMI and the other to LCD through ADV7513.

I've also read  About 1080p with LCD output on MX6Q and wanted to know if picture quality will be the same on both displays or LCD interface will produce worse picture?

In that thread there is information about poor LCD signal quality.

Is it still true? And if it is true will the upcoming SCM-i.MX6D resolve this issue?

Thanks!

0 Kudos
1 Reply

400 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yevhen

from theory point of view picture quality should be the same

but since such configuration was not tested on FSL reference boards,

it is not possible to say how it works in real application.

It may be suggested to ask people who performed such job on their boards.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos