KV1x and KV3x still there. So why KV4x was expelled? Does the Freescale dropped to put this chip into production?
Ari.
Hi Ari,
Because KV4x devices are updated during the preparation of KSDK 1.3 release, there will be a 1.3 based standalone version for KV4x device in the future, Thanks for your patience!
Have a great day,
Kan
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Kan,
Can you tell when the updated documentation and KSDK of the KV4x will be available? And when the KV4X will finally be in production?
Ari.
Hi Ari,
The Freescale Kinetis SDK_1.3.0 standalone for KV4x MCUs via TWR-KV46F150M is available on www.freescale.com . The Download button lead you to the Kinetis SDK Flexnet.
o Installers are in “KSDK v1.3.0 Standalone releases” item:
Installer: Kinetis SDK1.3.0 Standalone for KV4xF via the TWR-KV46F150M – Windows
Installer: Kinetis SDK1.3.0 Standalone for KV4xF via the TWR-KV46F150M – Linux
Installer: Kinetis SDK1.3.0 Standalone for KV4xF via the TWR-KV46F150M - Mac OS
MQX™ RTOS support for the TWR-KV46F150M Freescale Tower System module.
The Kinetis SDK is intended for use with Freescale’s Kinetis MCU product family based on the ARM Cortex-M series architectures. The release consists of:
o Kinetis MCU platform support
o Demo applications/Driver examples
o The FatFs FAT File System
o RTOS support components
o Documentation (Kinetis SDK API Reference Manual and various user’s guides)
Please consult the release notes.
Hope that helps,
Have a great day,
Kan
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------