Hi,
I am stuck with audio recording through MIC_IN in sabreauto_6q with android 5.0.2
we have tried to record through android sound Recorder app and tinycap.
1) In SoundRecorder app the needle is not deflecting... but the recording continues and onplay it plays silence
2)In Tinycap it captures few frames but on playback its complete silence
#tinycap /data/test.wav -d 1 -c2 |
Capturing sample: 2 ch, 44100 hz, 16 bit
Captured 577536 frames
Please help us with fix or debussing on above issue.
Other observation is recording through LINE_IN is successful and audio playback is also working.
Details on make configuration:
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=5.0.2
TARGET_PRODUCT=sabreauto_6q
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
TARGET_CPU_VARIANT=cortex-a9
TARGET_2ND_ARCH=
TARGET_2ND_ARCH_VARIANT=
TARGET_2ND_CPU_VARIANT=
HOST_ARCH=x86_64
HOST_OS=linux
HOST_OS_EXTRA=Linux-3.13.0-32-generic-x86_64-with-Ubuntu-12.04-precise
HOST_BUILD_TYPE=release
BUILD_ID=1.0.0-ga-rc4
OUT_DIR=out
environment set :
# setenv bootargs 'console=ttymxc3,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc3 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled'
#cat /proc/asound/cards |
0 [cs42888audio ]: cs42888-audio - cs42888-audio
cs42888-audio | |
1 [imxspdif | ]: imx-spdif - imx-spdif |
imx-spdif |
Thanks in advance ...
Hi Team,
My Build environment is below:
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=6.0.1
TARGET_PRODUCT=sabreauto_6q
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
TARGET_CPU_VARIANT=cortex-a9
TARGET_2ND_ARCH=
TARGET_2ND_ARCH_VARIANT=
TARGET_2ND_CPU_VARIANT=
HOST_ARCH=x86_64
HOST_OS=linux
HOST_OS_EXTRA=Linux-3.13.0-92-generic-x86_64-with-Ubuntu-14.04-trusty
HOST_BUILD_TYPE=release
BUILD_ID=1.0.0-ga-rc6
OUT_DIR=out
I connected electret microphone to the Mic in 1, With this I am able to record with below comand
#tinycap /data/local/tmp/test.wav -d 0 -r 48000 -c .
But the sound recorder app is silent. Please help me to get it enable.
Thank you in advance.
Rohit Kp####@@
Hi Experts,
Is any update on this for me, i am not able to make the mic up from Android. Please advise.
Thank you,
Rohit
according to the cs42888 driver, there is a PWR control. "ADC1" for AIN1/2, "ADC2" for AIN3/4. Please check the "ADC2" is switched on.
Hi Jimmychan,
Please advice how i can make ADC2 switch ON. I want make mic working through Android sound recorder App.
Please help me on this.
Thank You,
Rohit
Hi,
we could record and play successfully with 3 channels
#tinycap /data/local/tmp/test.wav -d 0 -r 48000 -c 3
But capturing with 1,2 ,4 channels are still silent.
Please suggest the changes required to capture with 1 channel.
Thanks for you reply.
Can you please guide on how to check "ADC2" is switched on