V3.2 , error"the codewarrior ide is licensed and a valid license key was not found "...feature:win32_cwide_limited.
Solved! Go to Solution.
Hi,
I've installed CW for M68K v3.2 on Win 7 64 bit OS and with the professional suite license, I can use the tool without problem.
What is the license file used ?
For this tool version, only the Professional Suite is available.
Attached you will find a temp license file.
This license file will expire the 15-nov-2015.
Rename the attached file to license.dat.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
To investigate the problem, we need to know exactly the CodeWarrior version you're using.
To do that you must:
Under CodeWarrior IDE (classic)
Start the IDE and click on Help | About Freescale CodeWarrior.
Click on Installed Products
Provide us all info displayed.
Or you can save them in a txt file.
If the Installed Products is not available for older version you should find information in the welcome.txt
under the installation folder.
What is the Windows OS Used ?
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
CodeWarrior for 68K Embedded Systems v3.2,
my OS is 64bit-win7。
in the “Obtaining Licenses ReadMe.txt” , there is the register E-mail "license@metrowerks.com",but it do not work.
:smileyconfused:first time to use the old version,thanks for help
Hi,
I've installed CW for M68K v3.2 on Win 7 64 bit OS and with the professional suite license, I can use the tool without problem.
What is the license file used ?
For this tool version, only the Professional Suite is available.
Attached you will find a temp license file.
This license file will expire the 15-nov-2015.
Rename the attached file to license.dat.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Done! thank you !