Hi,
I am using MPC8379 based processor board. If 120MB Memory test is performed using code warrior, it does not responding more than 5 hours. Afterwards 128MB is tested by splitting 16MB memory range. it was working.
Note: code warrior download algorithm is selected as target based.
1) How maximum memory range is possible to test at one shot?
2)whether MPC8379 is possible to test the memory using CW10.4?
Regards
Karunakaran R
Hello Karunakaran Radhakrishnan,
MPC8379 is not supported in CW PA 10.4, but I think you could try the workaround:
Try this and see if it's faster.
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------