P1010 DDR Controller Errata A-004508, Setting bit in mystery register to get Full Industrial Temperature Range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010 DDR Controller Errata A-004508, Setting bit in mystery register to get Full Industrial Temperature Range

814 Views
melbournebob
Contributor I

The P1010 Errata A-004508 states that bit 22 of a register at location 0x0_2f08 offset from the CCSR should be set if the controller is initialized below 0 degrees C and then operated at temperatures above 65 degrees C.

The P1010 Reference Manual has no definition of the register at 0x02f08 off the CCSR.  The largest offset for a DDR related register is at 0x02E58 (DDR_ERR_SBE).

When reading the mystery register I usually see 0x00000010, but occasionally I read 0x00000011.

Does anyone have a definition of the bits in this register (CCSR + 0x02f08)?  If I perform a read/modify/write to set bit 22 in this register will it cause any issues (even if the LSB is set)?

Note:  P1010 Chip Errata, Rev. L, 04/2013

Labels (1)
0 Kudos
Reply
2 Replies

552 Views
scottwood
NXP Employee
NXP Employee

Errata workarounds often reference undocumented registers.  If a workaround tells you to set or clear certain bits, use a read-modify-write.

0 Kudos
Reply

552 Views
alexander_yakov
NXP Employee
NXP Employee

The document you referring "P1010 Chip Errata, Rev. L, 04/2013" is not availably publicly, therefore it is not correct to discuss this document contents in public community.

Please enter a service request.

New Service Request

0 Kudos
Reply