Hi,
I built the images using 'bitbake core-image-minimal' and able to boot the EVM using SD Card. Now I am trying to boot the device using NFS.
But during the kernel boot, I was getting following errors:
*************************************************************************************************************
VFS: Mounted root (nfs filesystem) on device 0:12.
devtmpfs: mounted
Freeing unused kernel memory: 328K (80d13000 - 80d65000)
INIT: version 2.88 booting
Starting udev
udevd[124]: starting version 182
random: nonblocking pool is initialized
bootlogd: cannot allocate pseudo tty: No such file or directory
urandom start: failed.
Populating dev cache
/etc/rcS.d/S36udev-cache: line 33: /etc/udev-cache.tar.gz: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 86: /etc/volatile.cache.build: Permission denied
ln: /etc/resolv.conf: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 33: /etc/volatile.cache.build: Permission denied
/etc/rcS.d/S37populate-volatile.sh: line 56: /etc/volatile.cache.build: Permission denied
Tue Aug 4 10:34:42 UTC 2015
INIT: Entering runlevel: 5
Configuring network interfaces... ifup skipped for nfsroot interface eth0
run-parts: /etc/network/if-pre-up.d/nfsroot exited with code 1
Could not create /var/lib/dbus/machine-id.jUjbYd4v: Permission denied
Starting system message bus: dbus.
Starting syslogd/klogd: done
Poky (Yocto Project Reference Distro) 1.7 imx6slevk /dev/ttymxc0
imx6slevk login: root
Password:
Login incorrect
*************************************************************************************************************
The host PC is configured properly for NFS Server.
And the weird thing was, on login prompt when I entered username 'root', it was asking for the password. I am not able to understand why this is happening?
Please help me to resolve this issue.
Thanks,
Dhaval
Solved! Go to Solution.
Hi Dhaval,
I got the same problem with NFS boot. I added "no_root_squash" to host file /etc/exports. It works for me.
Good luck.
Bruce
Hi Dhaval,
I got the same problem with NFS boot. I added "no_root_squash" to host file /etc/exports. It works for me.
Good luck.
Bruce
Hi Bruce,
Thanks a lot for your help!That works for me too.. Can you please let me know, what does that option mean?
Thanks,
Dhaval
Hi Dhaval,
The is a good document about NFS permission problem. Please refer to 7. Troubleshooting section 7.4.
Regards,
Bruce
Thanks Bruce.
I see the filesystem was successfully mounted via nfs.
However it seems Linux on the board is unable to access many (or even all) files so it even unable to check root password.
Please make sure that nfs server is configured properly. Please check the permissions, etc.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------