I use the freescale http server. I have downloaded it on the freescale web site. I'd like to use the http post methode.
According to the header of the file "freescale_http.c"(part of the freescale http server), "The web server supports 'GET', 'POST','EMG'".
But int the header of the function freescale_process_header, it's written "We currently support GET and EMG.". In this function, there is no code corresponding to post. Does it mean that the post message is not actually available and will be soon available?
The POST comment is only a comment and the POST was not implemented but is on the "to-do" list.
We/Freescale are looking to implement some POST capability for handling the erase and program of the "dynamic flash file system". Hopefully we'll have an update to the code base in early February or sooner if possible.
You may like to take a look at the uTasker project. This supports the post method, including posting software uploads to the board.
The project is open source and completely free for non-commercial use - it is also fully supported and documented - see the web site www.uTasker.com and its forum at http://www.uTasker.com/forum/
Can you explain what the EMG method is? I haven't heard of this before.