prebuilt image for imx6qsabresd evaluation kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

prebuilt image for imx6qsabresd evaluation kit

624 Views
sachusanal
Contributor III

Hai  sir ,

could you please provide the link which i can download the prebuilt image of imx6qsabresd evaluation kit (which is provided by freescale when the board purchasing)

Board:IMX6QSABRESD Board

because  i need to test my sabresd board evaluation kit

please provide that one.

Labels (1)
0 Kudos
Reply
2 Replies

470 Views
igorpadykov
NXP Employee
NXP Employee

Hi sachu

demo images can be found on link below

L3.14.28_1.0.0_iMX6QDLS_BUNDLE  : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

470 Views
sachusanal
Contributor III

Hai Igor ,

Thanks for your response.

let me know in that link where i can find the demo image. i couldn't seen anything there...

please help me

0 Kudos
Reply