Hi,all
android L5.0.2 system build in my vmware ubuntu 12.04 LTS.
I met a android-L5.0.2 boot problem in my custom imx6dl board?
It is boot in sdhc0.
Using android_L5.0.0_1.0.0-ga_tools mfgtool burning.
I have not found the solution to the issues?
the logcat messages is below:
Freeing unused kernel memory: 340K (80e74000 - 80ec9000) | |
type=1403 audit(1.710:2): policy loaded auid=4294967295 ses=4294967295 |
type=1404 audit(1.720:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=42945
init: /dev/hw_random not found | |
Console: switching to colour dummy device 80x30 | |
init: /dev/hw_random not found | |
device-mapper: table: 254:0: verity: Data device lookup failed | |
device-mapper: ioctl: error adding target to table |
fs_mgr: Error loading verity table (No such file or directory)fs_mgr: Could no!
EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option |
EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: nomblk_ic
fs_mgr: __mount(source=/dev/block/mmcblk0p4,target=/data,type=ext4)=0 | |
EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option |
EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: nomblk_it
fs_mgr: __mount(source=/dev/block/mmcblk0p6,target=/cache,type=ext4)=0 |
EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk0p7,target=/device,type=ext4)=0 | |
init: cannot find '/system/bin/logd', disabling 'logd' | |
init: cannot find '/system/bin/lmkd', disabling 'lmkd' | |
binder: 108:108 transaction failed 29189, size 0-0 | |
init: cannot find '/system/bin/servicemanager', disabling 'servicemanager' | |
init: cannot find '/system/bin/vold', disabling 'vold' | |
init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger' |
init: using deprecated syntax for specifying property 'ro.serialno', use ${namd
init: using deprecated syntax for specifying property 'ro.product.manufacturerd
init: property 'ro.product.manufacturer' doesn't exist while expanding '$ro.pr'
init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/an'
init: using deprecated syntax for specifying property 'ro.product.model', use d
init: property 'ro.product.model' doesn't exist while expanding '$ro.product.m'
init: cannot expand '$ro.product.model' while writing to '/sys/class/android_u'
init: cannot find '/system/bin/netd', disabling 'netd' | |
init: cannot find '/system/bin/debuggerd', disabling 'debuggerd' | |
init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64' | |
init: cannot find '/system/bin/drmserver', disabling 'drm' | |
init: cannot find '/system/bin/mediaserver', disabling 'media' | |
init: cannot find '/system/bin/installd', disabling 'installd' |
init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'
init: cannot find '/system/bin/keystore', disabling 'keystore' | |||
init: cannot find '/system/bin/rild', disabling 'ril-daemon' | |||
init: cannot find '/system/bin/app_process', disabling 'zygote' | |||
init: cannot find '/system/bin/sh', disabling 'wifi_mac' | |||
init: cannot find '/system/bin/sdcard', disabling 'sdcard' | |||
init: cannot find '/system/bin/magd', disabling 'magd' | |||
android_usb: already disabled | |||
mtp_bind_config | |||
| |||
Who met this issuse? Or Anyone can give me some advices to solve the problem? | |||
The detail logcat message see attachment.
Thanks all, | |||
Leo | |||
Original Attachment has been moved to: log.txt.zip
Hi Carlos,
I try your method,but my bootimge must rebuild in my custom board. so I use android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz system.img.
And the same error with me.
But I also thank you for your advice?
Thanks,
Leo
HI,
yes,I use a Freescale BSP,android_L5.0.0_1.0.0-ga_core_source.gz.
How to solve this issues?
Thanks,
Leo
Hi,
It seems to be some confusion. Are you using mfgtool from Android 5.0.0_1.0.0-ga package to download a compiled image from Android 5.0.2?
The latest Android release provided by Freescale for i.MX6 series is L5.0.0_1.0.0, so, could you please verify if the mentioned error also happens when booting a precompiled image from the following package:
android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz
Hope this will be useful for you.
Best regards!
/Carlos
Hi all,
I found uboot should add bootargs environment: androidboot.selinux=disabled androidboot.dm_verity=disabled.
It will be boot success.
I don't know why?
Thanks,
Leo
Hi,
Are you using a Freescale BSP? Otherwise, the issue that you described may be caused by the following:
Validating SELinux | Android Open Source Project
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------