4 Channel 720P30 Video capture with single Soc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4 Channel 720P30 Video capture with single Soc

975 Views
shabbirlimdiwal
Contributor I

Hi,

For one of the upcoming products, we are looking for right architecture to implement SVM (Surround view monitoring) system. There will be 4 cameras mounted on car's front, rear, left and right side and we want to design a host system which can capture 4 channel Bayer/YUV data (each 720P@30), stitch them together to create one 720P view to be displayed on dashboard.

Can you suggest Freescale SoC which is able to capture 4 simultaneous channel 720P@30 fps?

If I am not wrong, one i.mx6 can capture two 720P30 channels at max. What if I want to capture 4 channels (I am fine using either CSI/paralle/both interfaces to achieve this use case).

If single SoC can't do that, what are the possible ways to achieve this use case?

Regards,
Shabbir

0 Kudos
Reply
1 Reply

501 Views
Yuri
NXP Employee
NXP Employee

In addition to Your previous thread You may look at the following :

"Surround View (D1) Demo on i.MX6"

https://community.freescale.com/docs/DOC-94541


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply