The board FRDM K64F use. Kinetis Design Studio IDE is being programmed. I receive a compile error when using the FXOS8700CQ in the component. Is there a workaround for this part?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The board FRDM K64F use. Kinetis Design Studio IDE is being programmed. I receive a compile error when using the FXOS8700CQ in the component. Is there a workaround for this part?

353 Views
youngsupark
Contributor I

The board FRDM K64F use.

Kinetis Design Studio IDE is being programmed.

I receive a compile error when using the FXOS8700CQ in the component.

Is there a workaround for this part?

 

25966_25966.JPG오류.JPG

Labels (1)
0 Kudos
1 Reply

247 Views
BlackNight
NXP Employee
NXP Employee

Hello,

are all the properties of the component configured? For example like this:

pastedImage_0.png

Erich

0 Kudos