Soldering Curve for P1020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Soldering Curve for P1020

660 Views
bfac
NXP Employee
NXP Employee

Hello,

Do we have soldering recommendation documents for P1020 QorIQ device?

The package is TEPBGA 689.

A customer had issues on the device soldering on their first prototypes (proven by X-Ray).

Thanks!

Bruno

Labels (1)
0 Kudos
Reply
1 Reply

544 Views
LPP
NXP Employee
NXP Employee

Please, refer to these documents:

http://cache.freescale.com/files/32bit/doc/package_info/PBGAPRES.pdf

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3300.pdf

http://www.freescale.com/files/product/doc/ENV_PBFREEOV2.pdf

Note. Package Peak Temperature (PPT) profile is for determination of components Moisture Sensitivity Level (MSL) and the parts’ processability per J-STD-020. PPT is the minimum temperature used for MSL qualification. Actual reflow temperature should not exceed this value. Optimal temperature profile depends on the solder paste and flux used.

The actual reflow profile to be used for any PCB should be available from the paste supplier as a recommended profile. Use care when looking at the paste reflow profiles supplied by paste vendors. Adjustments will have to be made when using a paste-flux for a set of conditions it is not primarily targeted for.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply