Hello friends,
I have following structure in the source code received from my vendor for MCF51EM256.
If not much of a trouble, will anybody please tell me whether this is a valid source code and if so, how to modify it in CodeWarrior?
<Folder>: Source_Code
<Folder>: Lib
<File>: mcf51em256.args
<File>: mcf51em256_c.d
<File>: subdir.mk
<File>: mcf51em256_c.obj
<Folder>: Project_Settings
<Folder>: Startup_Code
<File>: startcf.args
<File>: startcf_c.d !@
<File>: subdir.mk
<File>: startcf_c.obj
<Folder>: Sources
<File>: Main.args
<File>: Main_c.d
<File>: Main_c.obj
<File>: file_01.args
<File>: file_01_c.d
<File>: file_01_c.obj
:
:
<File>: file_32.args
<File>: file_32_c.d
<File>: file_32_c.obj
<File>: subdir.mk
<File>: file_x.args
<File>: file_x.elf
<File>: makefile
<File>: makefile.local
<File>: objects.mk
<File>: sources.mk
<File>: file_x.elf.S19
Solved! Go to Solution.
Hi,
you probably got just a project output directory which contains object code (*.obj) , makefile support files (*.mk), dependency files (*.d), compiler argument files (*.args)...
I'm afraid there is no source code present in this project structure.
regards,
Stan
Hi,
you probably got just a project output directory which contains object code (*.obj) , makefile support files (*.mk), dependency files (*.d), compiler argument files (*.args)...
I'm afraid there is no source code present in this project structure.
regards,
Stan
Hello Stan,
Many thanks for the reply.
As pointed out earlier, I'm afraid I was too naive not to know that I did not have the source code with me.
Best regards,
The project you got seems not built with CodeWarrior, I cannot find the link command file. What is the IDE used to build this project?
Fiona Kuang
Technical Information & Commercial Support
Hello Xin,
Many thanks for a prompt quick response.
I was naive enough not to be able to identify that the source code was not with me.
Best regards,