I renamed a project (say Project 2) and KDS kept creating .elf under previous name. So, I closed then deleted the project (not files just from KDS work space).
I tried to import Project2 thinking the KDS would create the .elf with Project2 name. However,..... when I try and import the Project2 KDS "sees" it, but "select box" for Project2 is in the background, I can't select it to import.
Any thoughts?
Regards,
Frank
User also needs to change the ‘Artifact Name’ option after rename the project in order to generate ELF with new name. To do it, please:
1) Click on ‘Project’ Menu-> Properties
2) Click on C/C++Build > Settings
3) Click on ‘Build Artifact’ tab
4) Change the name in ‘Artifact name’, please see the attached screenshot.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------