KDS2.0 Can't import previously Deleted Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS2.0 Can't import previously Deleted Project

355 Views
frankbannon
Contributor II

I renamed a project (say Project 2) and KDS kept creating .elf under previous name.  So, I closed then deleted the project (not files just from KDS work space).

I tried to import Project2 thinking the KDS would create the .elf with Project2 name.  However,..... when I try and import the Project2 KDS "sees" it, but "select box" for Project2 is in the background, I can't select it to import.

 

Any thoughts?

 

Regards,

 

Frank

Labels (1)
0 Kudos
1 Reply

275 Views
TICS_Fiona
NXP Employee
NXP Employee

User also needs to change the ‘Artifact Name’ option after rename the project in order to generate ELF with new name. To do it, please:

1) Click on ‘Project’ Menu-> Properties

2) Click on C/C++Build > Settings

3) Click on ‘Build Artifact’ tab

4) Change the name in ‘Artifact name’, please see the attached screenshot.


Artifact Name.png


Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos