I am running Yocto on board based on IMX6Q Soc. Everything till now is fine,but today I found an error when doing the video playback,this error happen and the video is too lag
Could anybody kindly give us any suggestion? Thanks in advance!
shell script :
export VSALPHA=1
gst-launch playbin2 uri=file:///home/root/1.mkv video-sink="mfw_isink axis-left=0 axis-top=0 disp-width=640 disp-height=480" &
gst-launch playbin2 uri=file:///home/root/2.mkv video-sink="mfw_isink axis-left=640 axis-top=480 disp-width=320 disp-height=240" &
top
here is the log message:
/home/grant/fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/libs/gst/base/gstbasesink.c(2875): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/MFW_GST_V4LSINK_INFO_T:mfw_gst_v4lsink_info_t0:
There may be a timestamping problem, or this computer is too slow.
WARNING: from element /GstPipeline:pipeline0/MFW_GST_V4LSINK_INFO_T:mfw_gst_v4lsink_info_t0: A lot of buffers are being dropped.
/home/grant/fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/libs/gst/base/gstbasesink.c(2875): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/MFW_GST_V4LSINK_INFO_T:mfw_gst_v4lsink_info_t0:
There may be a timestamping problem, or this computer is too slow.
WARNING: from element /GstPipeline:pipeline0/MFW_GST_V4LSINK_INFO_T:mfw_gst_v4lsink_info_t0: A lot of buffers are being dropped.
Hi Grant,
Did you try to use a different sink element, like mfw_v4lsink? Do you still have the same problem?
Regards,
Luca
Thanks for your reply!!!
I did use mfw_v4lsink instead,but the error still occour.
One thing I need to correct,
This issue is happend on IMX6 2 core version,On IMX6Q(4 cores),it is ok.
So I use IMX6Q now, this issue disappears.
I think this may be caused by performance difference。
Thanks!