BSP for HP Thin Clients?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP for HP Thin Clients?

1,858 Views
DarioC
Contributor I
Folks:
 
    Tried to download the BSP for HP Thin Clients from

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=012726006103321C8E - filled the questionnaire, SUBMIT - hit a 404. Already notified the webmaster and opened a support incident - which is still "Unassigned".

 

   Questions:

 

   1) Is anyone else using the BSP for HP Thin Clients? I'm just a hobbyst - got one for cheap from ebay (T5525) and plan to do some hacking with it

 

    2) Has anyone ever been able to download any BSP at all?

 

    Thanks !

 

    Dario

 

Labels (1)
0 Kudos
Reply
2 Replies

391 Views
Voxan
Contributor III
Hi there,

for what I can see, the page has been removed... The BSP is not available anymore.
FYI: this BSP was based on PCS which has been EOLed a while back.

Regards
0 Kudos
Reply

391 Views
DarioC
Contributor I
yep, page returns a 404 :smileysad:

I know the devices have been End-of-Sale by HP - but as I said, I'm just a hobbyst. I got one for cheap on ebay - I don't plan to mass-produce :smileyhappy:

Having the BSP would spare me the trouble of starting from scratch - I just want to download the BSP, not even asking for a SUPPORTED BSP :smileyhappy:

0 Kudos
Reply