I have p4080 pcie's demo board. and download QorIQSDK_02_03_00B_ltib.iso. I read P4080_PCIE_UG.pdf. It need P4080-PCIE-PRODUCTION-10-19-2011.tgz. but I can.t find the file . where is it? thanks.
I also need this file. Does anyone have it???
Use Please the QorIQ-DPAA-SDK-20110609-systembuilder.iso is "QorIQ DPAA SDK v1.0". It can be downloaded using the following link: https://www.freescale.com/webapp/Download?colCode=QorIQ_DPAA_SDK_v1.0&appType=license&location=null&....
See please the Release Note in the following file: http://www.freescale.com/lgfiles/NMG/NSD/P4080-PCIE-SDK-1.0-BINS-EP-05-03-2012.tgz
This Release Note is available in the attachment.
See also FAQ in the User_Manual_QorIQ_SDK_20110709.pdf. See attachment.
Load please the "P4080 PCIE SDK 1.0 Source code release" using the following link: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=P4080PCIE&nodeId=018rH325E40180&fpsp=... in Run-time Software item.
thank! but the wab address wasn't opened. https://www.freescale.com/webapp/Download?colCode=QorIQ_DPAA_SDK_v1.0&appType=license&location=null&...
Factory informed that this SDK is not available now. There is the following information from the factory.
We can not provide it anymore because it is not officially supported now.
Think you very much. I got the SDK from the other way, u-boot's log show " no link LTSSM=0x08, regs @ 0xfe200000" , pcie haven't scan the devices of the pcie's host bridge at the sametimes. But PCIE is good at the sametimes, u-boot's log show "LTSSM=0x16, x8, regs @ 0xfe200000 ", Would you help me?