Hi Devendra
This is the only registers that I have
See Attachments for more info
PMCTL Control Register Read/Write Section 11.10.1
PMFCTL Fault Control Register Read/Write Section 11.10.2
PMFSA Fault Status & Acknowledge Register Read/Write Section 11.10.3
PMOUT Output Control Register Read/Write Section 11.10.4
PMCNT Counter Register Read-Only Section 11.10.5
PWMCM Counter Modulo Register Read/Write Section 11.10.6
PWMVAL0-5 Value Register 0-5 Read/Write Section 11.10.7
PMDEADTM Deadtime Register Read/Write Section 11.10.8
PMDISMAP1 Disable Mapping Register 1 Read/Write Section 11.10.9
PMDISMAP2 Disable Mapping Register 2 Read/Write
PMCFG Configure Register Read/Write Section 11.10.10
PMCCR Channel Control Register Read/Write Section 11.10.11
PMPORT Port Register Read/Write Section 11.10.12
PMICCR Internal Correction Control Register Read/Write Section 11.10.13
Thanx