Hi Everyone,
While trying to interface 5MP MIPI (ov5640) with my custom sabresd board running on Android JB, encountered the following problem. The changes which I made in my init.freescale.rc didnt get reflected in the operation.
I added the following commands to my init.freescale.rc file,
setprop back_camera_name ov8825_mipi,ov5640_mipi,ov5640_camera,uvc
setprop back_camera_orient 0
insmod /system/lib/modules/ov5640_mipi.ko
But my logcat shows,
I/FslCameraHAL( 2301): Face Back Camera is 0, orient is 0
I/FslCameraHAL( 2301): Face Front Camera is 0, orient is 0
I tried all combinations of above commands within my init.freescale.rc but it didn work, Do I need to add these commands somewhere else?.
The above problem seems to be with ov5640 mipi only whereas ov8825 mipi and ov5640 paralled worked out well with the above combination.
Please download the Android FAQ.pdf.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
Under "Documentation"-->"Android"
The information you can find in the "22 How do I configure rear and front camera?"
Hope this can help you.