Read and write cycle delayed at the output of FTDI FT2232H

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read and write cycle delayed at the output of FTDI FT2232H

1,025 Views
jaymind
Contributor IV

Hello,

I used i.MX6Q and interfaced FTDI FT2232H in MPSSE mode on custom board, running it at 30MHz clock rate and Latency Timer is 255,

My FTDI FT2232H chip talk with ALTERA FPGA using SPI protocol.

I have downloaded libraries from below link and compiled with my App. code:

http://www.ftdichip.com/Support/SoftwareExamples/MPSSE/LibMPSSE-SPI/LibMPSSE-SPI_source.zip

I observe that the output signals show Read and Write transactions taking almost 3ms instead of few micro seconds.

On the code side the Read transactions take maximum 500us.

So, Is there any setting inside FTDI chip to decrease these timing delays or Do I need to choose another drivers ?

Regards

Jaymin D

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

771 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaymin

suggest to post this to ftdi support

FTDI Support

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

771 Views
jaymind
Contributor IV

OK.

Thanks...

0 Kudos
Reply