where can i find instruction for applying L3.0.101 BSP patch?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where can i find instruction for applying L3.0.101 BSP patch?

Jump to solution
4,514 Views
jaeminkim
Contributor I

hi there,

I'm trying to apply "L3.0.101_4.1.1_141016_source (I think this is some kind of patch)" to previous version of 3.0.35.

L3.0.101_4.1.1_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files. Size (K): 319113 Format: gz Rev #: L3.0.101_4.1.1. Modified: 11/3/2014

I couldn't find any instruction in gz archieve. please, can anyone help?

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
4,079 Views
Yuri
NXP Employee
NXP Employee

   Please refer to the next :

https://www.freescale.com/webapp/Download?colCode=IMX6LXPATCHRN&appType=license&location=null&Parent...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
4,080 Views
Yuri
NXP Employee
NXP Employee

   Please refer to the next :

https://www.freescale.com/webapp/Download?colCode=IMX6LXPATCHRN&appType=license&location=null&Parent...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,079 Views
yenchao
Contributor IV

Hi Yuri,

Is this link still available?

I need instruction for L3.0.101_4.1.1_141016_source too.

thx

0 Kudos
Reply
4,079 Views
Yuri
NXP Employee
NXP Employee

Please use the enclosed.

Yuri.

0 Kudos
Reply
4,079 Views
yenchao
Contributor IV

thank you!!

0 Kudos
Reply
4,079 Views
jaeminkim
Contributor I

Thank you!

0 Kudos
Reply