Dear All,
In our system, the external device is reset by using WDOG1 signal of i.MX6Solo.
When WDOG time-out occurred, we want to reset an external device by making GPIO_19 to Low by software.
Does such a usage have any problem?
If no problem,
Would you advise it about the setting method?
Or should WDOG1_B signal be used?
(from DISP0_DAT8 pad or GPIIO_9 pad or SD1_DATA2 pad)
May I have advice?
Best Regards,
Yuuki
Solved! Go to Solution.
Hi yuuki
one can use wdog interrupt and toggle GPIO_19 by software
in wdog interupt routine, this is described in sect.70.4.8 Interrupt IMX6DQRM
WDOG1_B resets processor, so I would not recommend to use it for such
task.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yuuki
one can use wdog interrupt and toggle GPIO_19 by software
in wdog interupt routine, this is described in sect.70.4.8 Interrupt IMX6DQRM
WDOG1_B resets processor, so I would not recommend to use it for such
task.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------