Hello,
I use Kinetis Design Studio V2.0.0.My cpu conf. like this:
I'm using FRDM KL25 dev board for USBDM debugger. When I load program with USBDM flash programmer, nothing happened but in debug mode its working. What is the wrong? Thanks.
Hi Gokhan,
1) The USBDM is open to everyone, so the USBDM from different company have a little difference ,
it usually used to CW, you should be sure whether yours can used to KDS.
2) In the FRDM-kl25 board , you can directly flash through the openSDA , it only need link use USB. You can try .
Best Regards
Alice
Thanks Alice,
I'm not using FRDM-kl25 board to develope, only using to programming extenal device. My custom board has MKL02Z32VFK4.