ETA on KSDK support for TWR-KL25Z48M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETA on KSDK support for TWR-KL25Z48M?

475 Views
andersop
Contributor I

As far as I can tell, TWR-KL25Z48M is not yet supported by KSDK 1.1.0 (using KDS 2.0.0).

 

Any timeline on when this will be available?

 

Currently it seems that there is no source-level project available for this board using KDS/GCC (the only packages I have found which do contain source are either for CW or are set up for another compiler.) I am currently trying to get a project building with Processor Expert but it would be nice to have a fully supported official package to start from.

Labels (1)
Tags (3)
1 Reply

392 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi phil,

kl25 should be supported in KSDK 1.2GA, and it will be available in Apr.2015

Best Regards,

Zhang Jun

============================================

this answer is for you, if it helps, please click on "Correct Answer " button. thanks!